FUNCTION_BLOCK CrossProduct
This function will calculate the Cartesian product (outer product) of two vectors
. The result will be returned in vector
.
Keep in mind that, due to rounding errors, the input of two collinear vectors will not necessarily result in the null vector.
| InOut: |