FUNCTION ProjectPointOnLine : BOOL
This function will project the point
onto a straight line: thereby, the direction vector of the straight line is taken as normal vector of a plane that is moved along the line as long as it touches the point
. The intersection point of the plane with the line corresponding to this location is the projected point.
| InOut: |