SubVector (FUN)

FUNCTION SubVector : BOOL

This function will subtract two input vectors and store the result within vector :

InOut:

Scope

Name

Type

Comment

Return

SubVector

BOOL

The return value is not used.

Input

pv1

POINTER TO Vector3d

Pointer to input vector

pv2

POINTER TO Vector3d

Pointer to input vector

pv

POINTER TO Vector3D

Pointer to output vector