Read (FB)

FUNCTION_BLOCK Read EXTENDS CBM.ETrigToA

Function block to read data from the serial port

InOut:

Scope

Name

Type

Comment

Inherited from

Input

xExecute

BOOL

Rising edge: Action starts

Falling edge: Resets outputs

If a falling edge occurs before the function block has completed its action, the outputs operate in the usual manner and are only reset if either the action is completed or in the event of an error. In this case, the corresponding output values (xDone, xError) are present at the outputs for exactly one cycle.

ETrigToA

xAbort

BOOL

TRUE: Action is stopped immediately and all outputs are reset to their initial values.

ETrigToA

udiTimeOut

UDINT

Defines the time (µs) after which an FB (e.g. requiring an external acknowledgement) aborts operation due to a timeout with error message.

ETrigToA

Output

xDone

BOOL

TRUE: Action successfully completed

ETrigToA

xBusy

BOOL

TRUE: Function block active

ETrigToA

xError

BOOL

TRUE: Error occurred, function block aborts action

FALSE: No error

ETrigToA

xAborted

BOOL

TRUE : Action aborted by user

ETrigToA

Input

hCom

CAA.HANDLE

Handle to the open COM port. Ist returned by the COM.Open function block.

pBuffer

CAA.PVOID

Pointer to a buffer to get the received data from the COM port

szBuffer

CAA.SIZE

Maximum size of the pBuffer parameter in bytes

Output

eError

ERROR

Local library error ID (0: no error; 5001: time out)

szSize

CAA.SIZE

Returns the number of received data bytes in pBuffer