INTERFACE ITimingController EXTENDS __SYSTEM.IQueryInterface
Applied whenever the timing related behaviour needs to be checked, for example, if a specific time limit is required.
Properties:
ControllerTimeLimit
ControllerTimeOut
CurrentControllerTime
Methods:
ControllerCheckTiming
StartInvocationTimer
StartOperationTimer
Structure: