RemoteAdapter_diag.CheckSupportedCommunicationState (METH)

METHOD CheckSupportedCommunicationState : BOOL

This method checks if a specific DEVICE_TRANSITION_STATE is supported by the node in general.

Note

Use IDevice2.CheckCurrentSupportedCommunicationState to check which DEVICE_TRANSITION_STATE is possible in the current state.

InOut:

Scope

Name

Type

Comment

Return

CheckSupportedCommunicationState

BOOL

True if node supports the requested DEVICE_TRANSITION_STATE in general.

Input

eRequestedState

DEVICE_TRANSITION_STATE