class
IScriptApplicationDownloadIds.
IScriptApplicationDownloadIds
Bases: object
The combination of code_id and data_id is a unique identifier of a application that is running on the controller. To find the source project that matches this application these values are stored in the *.project file.
code_id
The code_id.
Guid
data_id
The data_id.