SMC_BlockSearch (FB)

FUNCTION_BLOCK SMC_BlockSearch

This function block shortens the path from start up to the position that is stored in SMC_BlockSearchPos. From this position, the original path is put on. SMC_BlockSearch runs in the context of path preprocessing and is typically inserted right before SMC_CheckVelocities.

Note

SMC_BlockSearch requires the position values from SMC_BlockSearchSavePos, which must have been executed before.

Note

The element to restart with is identified by its sourceline number. So, there will be ambiguities when dealing with subprograms (we will restart with the first element holding the correct sourceline number, which, in general, is part of the main program).

InOut:

Scope

Name

Type

Comment

Inout

ePos

SMC_BlockSearchPos

Position information. Requires connection to output ePos of SMC_BlockSearchSavePos

Input

bExecute

BOOL

Risign edge: Enables the function block

bAbort

BOOL

TRUE: Aborts the processing of the function block

bAppend

BOOL

FALSE: Starts emptying poqDataOut on a rising edge at bExecute

poqDataIn

POINTER TO SMC_OUTQUEUE

Pointer to data of structure SMC_OUTQUEUE containing the path objects of typ SMC_GEOINFO, that are interpolated.

bStartFromSavedPos

BOOL

TRUE: Enables the function block to shorten the path from start up to the position, that is stored in SMC_BlockSearchPos .

FALSE: Disables the function block

nSizeOutQueue

UDINT

Size in bytes of the data buffer pbyBufferOutQueue, in which the path elements are copied. If the value is set, it may not be changed except after a reset.

pbyBufferOutQueue

POINTER TO ARRAY [0..0] OF SMC_GEOINFO

Pointer to the first byte of the storage area created for the path elements. If the value is set, it may not be changed except after a reset.

Output

bDone

BOOL

TRUE: input date from poqDataIn have been precessed fully. After that, the function block performs no action until a reset is detected. When bExecute is set to FALSE, bDone is reset to FALSE.

bBusy

BOOL

TRUE: Function block in execution

bError

BOOL

TRUE: Error has occurred

wErrorID

SMC_ERROR

Error identification

Possible values

  • SMC_BS_SAVEDPOS_NOT_REACHED: Stored position has not been found. Probably wrong path.

  • SMC_BS_NO_POS_STORED: ePos contains no stored position. Possible cause is that SMC_BlockSearchSavePos was not executed or in a wrong way.

poqDataOut

POINTER TO SMC_OUTQUEUE

Pointer to data of structure SMC_OUTQUEUE containing the path elements of type SMC_GEOINFO that have been processed

Structure: