Printf (FUN)

FUNCTION Printf

This function performs a “formatted printing” of the value <pValue> points to.

InOut:

Scope

Name

Type

Comment

Input

cbsResult

REFERENCE TO CharBufferString

The buffer, where the result will be returned

cbsFormat

REFERENCE TO CharBufferString

The format string used for formatting the value

pValue

POINTER TO BYTE

A pointer to the begin of the piece of memory, where the value to format is stored.

typeClass

__SYSTEM.TYPE_CLASS

A __SYSTEM.TYPE_CLASS value describing the type of the value to format