Configuration

 

Overview of Configuration Steps

Configuration Steps

The following sections provide information on the process of setting up a Sercos bus, adding devices, configuring the network communication, configuring the individual devices, and commissioning the system with EcoStruxure Machine Expert Logic Builder.

Refer to the ATV340S Hardware Guide for information on installation and wiring.

Step

Action

1

Add a Sercos master

2

Add Sercos slaves

3

Configure the Sercos cycle time

4

Configure the Sercos communication

5

Configure the Ethernet communication

6

Configure simulated slaves

7

Configure the parameters of a drive for cyclic communication

8

Configure devices via the service channel