AlarmStateTransition (ENUM)

TYPE AlarmStateTransition :

This enumeration defines the possible state changes an alarm can have.

InOut:

Name

Initial

Comment

NoTransition

0

Value signals, that there is no alarm state transition

Pending

-1

An inactive alarm is going to be pending (alarm condition is true, but alarm is not yet active).

Activate

1

An inactive (resp. pending) alarm is going to be active (alarm condition is true).

Deactivate

2

An active alarm is going to be inactive (alarm condition is no longer true).

Acknowledge

3

Alarm is still active and will be acknowledged.

Confirm

4

Alarm is no longer active and will be confirmed.