FUNCTION ConvertTimestampToLDateAndTime : LDATE_AND_TIME
This function converts the alarm time stamp from type timestamp into the LDATE_AND_TIME type which can be monitored in a better readable way.
Scope
Name
Type
Comment
Return
ConvertTimestampToLDateAndTime
LDATE_AND_TIME
Input
timestamp
Timestamp
iOffset
INT
UTC Offset (-1 = Still use convert to local time)