IAlarm.GetMessage (METH)

METHOD GetMessage : CharBufferPtr

Returns the message text, that has been configured for the alarm. The result is a pointer to the buffer, where the message text is stored

InOut:

Scope

Name

Type

Comment

Return

GetMessage

CharBufferPtr

Input

stringType

__SYSTEM.TYPE_CLASS

A __SYSTEM.TYPE_CLASS indicating, which type of string has to be retrieved