Internal

All functions in this folder are unmanaged functions. No resource manager is managing the resources. This means that the caller is responsible for freeing all resources (Prefix “_”). Functions without resource manager have better performance. Handles returned by unmanaged functions should not be used with managed functions and vice versa.