CAA Can Low Level Extern Library Documentation

Company

CAA Technical Workgroup

Title

CAA Can Low Level Extern

Version

3.5.17.0

Categories

Intern|CAA|Fieldbus

Namespace

CL2

Author

3S - Smart Software Solutions GmbH

Placeholder

CAA CanL2

Description [1]

Hardware abstraction layer for CANbus systems (Network Level 2). Note: If RTS_SIL2 is defined, all used resources are unmanaged even if managed functions are used.

Indices and tables

[1]

Based on CAA Can Low Level Extern.library, last modified 20.04.2021, 14:31:08. LibDoc 4.0.0.0

The content file CAA Can Low Level Extern.clean.json was generated with CODESYS V3.5 SP16 Patch 3 on 20.04.2021, 14:31:09.