DirRename (FB; Prefix fildrn)

FUNCTION_BLOCK DirRename EXTENDS CBM.ETrig

This function block can be used to rename a directory and is optional for the different targets.

Contrary to the original CAA specification the directory may be renamed even if it is opened via ”FILE.DirOpen”.

This behavior is dependent of the underlying operating system and file system.

Whether this function block is implemented or not is explicitly stated and encoded in the return value of the function ”FILE.GetProperty”.

It is not recommended to use this function block to move files (it may work but is system dependent). Please use the appropriate function block ”FILE.Rename” instead.

InOut:

Scope

Name

Type

Comment

Inherited from

Input

xExecute

BOOL

Rising edge: Action starts

Falling edge: Resets outputs

If a falling edge occurs before the function block has completed its action, the outputs operate in the usual manner and are only reset if either the action is completed or in the event of an error. In this case, the corresponding output values (xDone, xError) are present at the outputs for exactly one cycle.

ETrig

Output

xDone

BOOL

TRUE: Action successfully completed

ETrig

xBusy

BOOL

TRUE: Function block active

ETrig

xError

BOOL

TRUE: Error occurred, function block aborts action

FALSE: No error

ETrig

Input

sDirNameOld

CAA.FILENAME

Old directory name

sDirNameNew

CAA.FILENAME

New directory name

Output

eError

ERROR

Local library error ID (0: no error; 5101: time out)