CAA Technical Workgroup
CAA File
3.5.19.0
Intern|CAA|System
FILE
3S - Smart Software Solutions GmbH
CAA File
This library provides function blocks for accessing file directory systems and files. The standardized inputs and outputs of the function blocks are described in detail in the CAA Guidelines and will therefore not be described here. File access is only supported in binary mode. All input values of the function blocks are stored in local internal variables. This does not apply for the contents of memory structures where a pointer is passed on as an input for example “pBuffer“ of “FILE.Read“ or “FILE.Write“.
CAA.FILENAME which is described in “CAA_Types.library“ should be usable for library “CAA_File“ in the following way. Separators between directory paths in “CAA.FILENAME“ are the slash („/“) or the back-slash („\“). The interpretation of the directory path is tolerant to the effect that either one or the other of these characters can be used.
Mixed usage should be avoided by an error message. The part of a “CAA.FILENAME“ character string behind the last separator is the file name. The rest specifies the directory path. Only in the first part of the directory path may a series of colons be used for the specification of drive letters or for device identification. The function block FILE.SetRoot provides for an enhanced portability of the applications, regardless of the many different options available to display a directory path. The starting point within the directory tree can thus be set centrally and it is then possible to navigate through the application relative to this starting point.
Absolute paths in the local file system:
C:/dir/Test.txt or /ram:2/home/Test.txt
Relative paths in the local file system:
../Log/Test.txt or Log/Test.txt
Complete path specification for a file in the local files system:
file://C:/dir/Test.txt
(if supported by the current system) Complete path specification for a file on a FTP Server:
ftp://<user>:<passwd>@<ip-addr>[:<port>]/home/user/Test.txt
(if supported by the current system) Complete path specification for a file on a HTTP Server:
http://<ip-addr>[:<port>]/dir/Test.txt
Whether the appropriate resolver functions for FTP- or HTTP- Servers are available in the corresponding implementation, can be evaluated via function FILE.GetProperty. Only IP addresses are valid, the resolution of a name is not intended for in the functional scope of the library “CAA.File“.
The resource management within the library is done by two function blocks in the global variable list RSHandling.
g_FileClass for managing file handles.
g_DirClass for managing directory handles.
The key data for the management of the resources can be set via the Reset method.
myAsyncProperty : RSU.AsyncProperty;
myPoolExtender : RSU.PoolExtender;
myAsyncProperty := RSU.g_AsyncProperty;
myAsyncProperty.usiTaskPrio := 30;
myAsyncProperty.tnTaskName := 'myPoolExtender';
myPoolExtender.Reset(myAsyncProperty);
FILE.g_FileClass.Reset(
udiInitialPoolSize := 40 * SIZEOF(__XWORD),
udiNumExtensionBlocks := 20,
itfPoolExtender := myPoolExtender;
);
If udiNumExtensionBlocks and itfPoolExtender is set to zero no memory expansion of the resource management is done.