Input
|
xExecute
|
BOOL
|
Rising edge: Action starts
Falling edge: Resets outputs
If a falling edge occurs before the function block has completed its action, the outputs operate in the usual manner and are only reset if either the action is completed or in the event of an error. In this case, the corresponding output values (xDone, xError) are present at the outputs for exactly one cycle.
|
ETrig
|
Output
|
xDone
|
BOOL
|
TRUE: Action successfully completed
|
ETrig
|
xBusy
|
BOOL
|
TRUE: Function block active
|
ETrig
|
xError
|
BOOL
|
TRUE: Error occurred, function block aborts action
FALSE: No error
|
ETrig
|
Input
|
hFile
|
CAA.HANDLE
|
File handle
|
|
udiPos
|
__UXINT
|
Offset position, Number of bytes from the start of the file
|
|
Output
|
eError
|
ERROR
|
Local library error ID (0: no error; 5101: time out)
|
|