CAA Technical Workgroup
CAA Mathematics
3.5.19.0
Intern|CAA|Utilities
MATH
3S - Smart Software Solutions GmbH
Some basic functions for handling problems out of the mathematic domain
Functions
Global Variables
Structs
GetSupplierVersion (Function)
Library Information
GetLibVersion (Function)
GetLibVersionNumber (Function)
IsLibReleased (Function)
VersionConstants (GVL)
[1]
Based on CAA Mathematics.library, last modified 02.03.2023, 10:44:34. LibDoc 4.0.0.0
The content file CAA Mathematics.clean.json was generated with CODESYS V3.5 SP16 Patch 3 on 02.03.2023, 10:44:36.