Symbols

Every object has a status in the index (staged changes) and in the Git repository. The status is displayed by a corresponding symbol before the object in the navigator views of the CODESYS project or in the Status & Staging view.

Symbol

Description

Unaltered (in the working directory)

The object is unchanged from the index.

Modified (in the working directory)

The object has been changed from the previous version in the index.

New (in the working directory)

The object exists in the working directory, but it is not yet in the index or local repository.

Conflict

A conflict occurred when merging the object.

Deleted (in the working directory)

The object does not exist in the working directory, but it still exists in the index.

Error

No assignment to a status

The symbol is displayed only in the navigator.

Transient

Transient objects are not applied to the Git repository. The symbol is displayed only in the navigator.

The Git status could not be determined yet. As soon as the status is known, the corresponding symbol is displayed. The symbol is displayed only in the navigator.