Symbol:
Corresponding Git command: git branch
Function: The local Git branches are displayed and managed in the view. These can be branches which are already tracking a remote branch, or branches which exist purely locally and do not contain any link to a remote repository.
Call: Git → Branches menu
Requirement: At least one commit exists in the repository.
|
The view is refreshed. |
|
|
Opens the Create New Branch dialog to create a new local branch as a copy of the currently selected local branch (see above) |
|
|
The selected branch is deleted, even if the branch has not yet been merged completely. Note: The current branch cannot be deleted. |
|
|
As a result of the A checkout is prevented by uncommitted changes. When dealing with a remote branch – an entry under Remote (<n>) – the following options are possible:
|
|
( |
Clicking the button will execute the command directly. Alternatively, you could also set options for it. To do this, use the When you confirm the request (dialog prompt) whether or not you really want to commit, the commits of the currently selected branch are committed to the current branch. The current branch is the one whose status is now in the working directory. (check mark in the Current column) If conflicts occur while merging, then they have to be resolved first. Depending on the case and the set merge Options, automated actions will run or manual actions are necessary. If a conflict cannot be resolved automatically, then this is indicated in the Git Status & Staging view. For conflict resolution in the first step, pay attention to the context menu commands provided in the Status & Staging view. Also see the Merge Conflicts help page.
As long as the merge operation has not been completed, the status info |
|
|
Opens the Set upstream remote for Branch dialog Here a branch corresponding to the local branch is created and the link with it set up on the linked remote repository (usually named "origin" and located on a server, for example). |
|
|
Opens the Track a remote branch dialog Here the local branch can be linked with an available representative of a remote repository (remote branch). This allows for an exchange of commits (Git operations Pull and Push) between the local repository and remote repository. |
|
( |
The status of the tracked remote repository branch is fetched in the local branch ( |
|
( |
If the selected branch is not a tracking branch, then the Push Branch dialog opens. Here you specify the remote branch to be merged into. The commits of the local branch are copied to the corresponding branch in the remote repository. If the selected branch is a tracking branch, then the action is performed immediately. No dialog opens. |
|
Compare |
The selected commit is compared with the last state of the object in the project storage and changes are displayed in the comparison view. When two commits are selected, they are compared. |
|
Filter branches: Local|Remote |
By clicking the Local (<n>) and/or Remote (<n>) buttons, the display of local branches and/or remote branches ("representatives" of the branches located in the remote repository) is enabled or disabled in the table. |
|
Table |
Current:
Remote:
Tracking: Name: Name of the branch Canonical name: Unique name of the branch
Example:
Remote: Name of the remote repository which the remote branch references (usually Upstream branch canonical name
Example: Tracked branch name: Name of the remote branch which is tracked
Example:
Tracked branch canonical name: Canonical name of the remote branch which is tracked. Example: When a branch tracks a remote branch, the following information is relevant. Attention: This display is refreshed only when a Fetch command is executed: Commits ahead: Number of commits on the local (tracking) branch with which its time is "ahead" of the remote branch Commits behind: Number of commits on the local (tracking) branch with which its time is "behind" the remote branch |