When buffered movements or blending movements are commanded, the function block instance that commands the subsequent movement must not be executed earlier than the function block instance that commanded the previous movement.
If this order is violated, then the new error SMC_MOVING_WITHOUT_ACTIVE_MOVEMENT
is reported and the axis switches to the state Errorstop
.