You can set the offset between the flange coordinate system of the kinematics (XYZ) and the TCP coordinate system of the kinematics (X'Y'Z') by means of configuring a tool offset. This tool offset acts on all subsequent movements.
TCP: Tool Center Point
The tool offset is specified by a shift v=(x,y,z) and a rotation r=(A,B,C) in ZYZ Euler angles. Shift and rotation are expressed relative to the flange coordinate system of the kinematics.
When you configure a tool offset, it can be incompatible with the current kinematics. As a result, a tool offset can cause the kinematics to be incapable of achieving orientations. In this situation, an error is issued and the tool offset is ignored. For example, you can configure a tool offset in the Z-direction for the kinematics Kin_Scara2_Z. On the other hand, an offset with parts in the X- or Y-direction results in an error. When kinematics have these kinds of restrictions, they are described with the kinematics.