In the device tree, select an application.
Click Project → Add Object → Alarm Configuration to insert an alarm configuration.
The Alarm Configuration object is displayed below the application in the device tree.
The alarm configuration already has the predefined Error, Info, and Warning alarm classes, as well as the AlarmStorage object. It is helpful to use the predefined objects. You can also create your own objects.