Function: The dialog lists the installed symbol libraries and allows you to assign symbol libraries to a project.
Call: Project → Project Environment menu, Visualization Symbols tab
Requirement: The open project contains a visualization and has been saved with a compiler version less than 3.5.7.0
. Symbol libraries are known in compiler version 3.5.7.0
and higher.
Symbol library |
List of all installed symbol libraries |
Active |
|