Symbol:
Category: Special Controls
The element displays the curve of variable values as a trend diagram. The trend diagram is suitable for representing a long-term data curve because the data is read from a trend recording and hence from a database. Moreover, you can run the Trend element together with the Date Range Picker, Legend, and Time Range Picker operating elements so that the user can navigate conveniently in the diagram.
You can programmatically delete the recorded trend curve at runtime. The recording starts again from the time of deletion.
For more information, see: Programming a Trend Visualization
| NOTICE | |
|---|---|