Symbol:
Category: Special Controls
The element graphically displays the curve of array values as a line or bar chart in the Cartesian coordinate system. The chart can display multiple curves at one time.
Constraint
The element can be used with controller with V3.5 SP11 and higher.
NOTICE | |
---|---|