Image

Static ID

Reference to the image of an image pool according to the following the scheme:

<name of image pool>.<image ID>

Example: Imagepool.GreenButton

If the image is from the GlobalImagePool, then you can omit the name of the image pool because this pool is automatically searched first.

: The Input Assistant dialog opens and lists all available image pools and images in the entire project.

Scale type

Behavior of the image when resizing the button.

  • Isotropic: The image retains its proportions. The ratio of height to width is retained, even if you change the height or width of the button separately.

  • Anisotropic: The image resizes to the dimensions of the button.

  • Fixed: The image retains its original size, even if you resize the button.

Transparency

The visualization displays the image with the transparency color that is selected in Transparency color.

Transparent color

Requirement: The Transparency option is selected.

Color which is transparently in the image

Example: White

If the image background that is reference by Static ID is white, then this background is displayed transparent.

Clicking opens a color picker dialog.

Horizontal alignment

Horizontal alignment of the image

  • Left

  • Centered

  • Right

Vertical alignment

Vertical alignment of the image

  • Top

  • Centered

  • Bottom