RALARM_MODE (ENUM)

TYPE RALARM_MODE :

Filter scope of RALARM.F_ID input.

Attributes:

qualified_only

InOut:

Name

Initial

Comment

ALL_ALARMS

1

If the Host Controller interface has received an alarm, all function block outputs are updated. The alarm is acknowledged.

ALARM_BY_ID

2

Receive an alarm for the slot or subslot the identification of which is given in F_ID input, all function block outputs are updated. The alarm is acknowledged

ALARM_BY_SLOT

3

Receive an alarm for the slot the identification of which is given in F_ID input AND for all of it’s subslots

ALARM_BY_DEVICE

4

Receive an alarm for the device the identification of which is given in F_ID input AND for all of it’s slots and subslots