FUNCTION_BLOCK Start EXTENDS BaseService
This function block is used for calling the “Start” service of a specific instance of a CIP object. The exact effect of this service depends on the CIP class (refer to the CIP specifications (Vol. 1 and 2).
|
InOut:
|
|
Scope
|
Name
|
Type
|
Comment
|
Inherited from
|
|
Input
|
xExecute
|
BOOL
|
Rising edge: Action starts
Falling edge: Resets outputs
If a falling edge occurs before the function block has completed its action, the outputs operate in the usual manner and are only reset if either the action is completed or in the event of an error. In this case, the corresponding output values (xDone, xError) are present at the outputs for exactly one cycle.
|
ETrig
|
|
Output
|
xDone
|
BOOL
|
TRUE: Action successfully completed
|
ETrig
|
|
xBusy
|
BOOL
|
TRUE: Function block active
|
ETrig
|
|
xError
|
BOOL
|
TRUE: Error occurred, function block aborts action
FALSE: No error
|
ETrig
|
|
Input
|
itfEtherNetIPDevice
|
IEtherNetIPService
|
|
BaseService
|
|
eClass
|
CIPClass
|
|
BaseService
|
|
dwInstance
|
DWORD
|
|
BaseService
|
|
Output
|
eError
|
ERROR
|
|
BaseService
|
|