FloorF (FUN)

FUNCTION FloorF : REAL

Returns the greatest integral value that is not greater than f. If f is +0, -0, infinity, or NaN, then f is returned.

InOut:

Scope

Name

Type

Input

f

REAL

Return

FloorF

REAL