Speed Select

 

Overview

This part explains the functionality and implementation of the SpeedSelect function block in the Hoisting Library.

What Is in This Part?

This part contains the following chapters:

oSpeedSelect: Provides the Option to Choose between 8 Predefined and one Analog Speed