Aliases

 

Aliases

Overview

Type:

ALIAS (DUT)

Available as of:

V1.0.0.0

Inherits from:

Description

An alias represents a complex data type which is used in this library.

Name

Data type

Description

DiagTable

ARRAY [0..GPL.Gc_uiMaxNumOfDiagEntries - 1] OF ST_DiagMessage

Data type of the data table which is used to store the diagnostic messages.