Complete (Method)

Overview

Type:

Interface

Available as of:

V1.4.2.0

Inherits from:

Description

The method represents the state Complete (17) from the PackML state model.

Interface

Intput

Data type

Description

i_xIsFirstCycle

BOOL

Indicates if this is the first time the state method is invoked.

i_ifCommands

IF_StateCommands

Provides access to the state commands. This allows you to trigger a command from inside the state method.

i_ifUnitMode

IF_UnitMode

Provides information about the unit control mode.