ST_Ingredients

Overview

Type

Data structure

Available as of

V1.4.2.0

Description

The structure ST_Ingredients is a collection of tags providing information for the recipe ingredients.

Structure Elements

Variable

Data type

Description

Parameter_REAL

ARRAY [1.. GPL.Gc_uiNumOfParamREALRecipeIngredients] OF ST_Parameter_REAL

Structured array of ingredient information for values with REAL data type

Parameter_STRING

ARRAY [1.. GPL.Gc_uiNumOfParamSTRINGRecipeIngredients] OF ST_Parameter_STRING

Structured array of ingredient information for values with STRING data type

Parameter_LREAL

ARRAY [1.. GPL.Gc_uiNumOfParamLREALRecipeIngredients] OF ST_Parameter_LREAL

Structured array of ingredient information for values with LREAL data type

Parameter_DINT

ARRAY [1.. GPL.Gc_uiNumOfParamDINTRecipeIngredients] OF ST_Parameter_DINT

Structured array of ingredient information for values with DINT data type

Used By

  • ST_Recipe