Output for signaling the active ramp monitoring for the requested safety-related monitoring function(s).
Ramp monitoring can be parameterized for the following safety-related monitoring functions:
Data type: SAFEBOOL
Connection: If required, the signal can be connected to a variable of the SAFEBOOL data type or to other safety-related functions/function blocks for further processing or evaluation.
Value |
Description |
---|---|
SAFETRUE |
If ramp monitoring is active, the deceleration curve is monitored during the t2 interval and must follow the parameterized ramp. Otherwise, the fallback function defined for the corresponding safety-related function is activated. |
SAFEFALSE |
If ramp monitoring is not active, the deceleration curve is not monitored during the t2 interval. Even acceleration is allowed in the ramp-down phase. The safety-related function must be executed correctly the latest before t2 elapses. Otherwise, the fallback function defined for the corresponding safety-related function is activated. |