METHOD GetRecipeVariableNames : DWORD
Returns the recipe variable names from the corresponding recipe
Example:
We have 50 recipe variable names. We want to create a table which shows 10 recipe variable names at the same time. We define a string array strArr: ARRAY[0..9] OF STRING; Corresponding to the iStartIndex we can get the recipe variable names from a specific area.
StartIndex := 0; The variable names 0..9 are returned.
iStartIndex := 20; The variable names 20..29 are returned.
In this example:
iSize := 10;
InOut: |
|