RecipeManCommands.SetStoragePath (METH)

METHOD SetStoragePath : BOOL

Sets the storage path of the recipe management dynamically

It overrides the storage path which is normally configured in the recipe manager configuration.

InOut:

Scope

Name

Type

Comment

Return

SetStoragePath

BOOL

TRUE, if the storage path was set successfully.

Possible error reasons are:

See ReturnValues (GVL) for a description of all possible errors.

Input

stPath

STRING(512)

The storage path i.e. c:/recipes/