IScriptProjectExtension

class

IScriptProjectExtension.

IScriptProjectExtension

Bases: object

Provides extensions for IScriptProject

code_analysis

Access to code_analysis scripting API.

reset_memory_reserve_for_online_change

Resets the memory reserve for online change of function blocks in the pool.

finish_load_project

Directs that a project is loaded completely.

is_project_load_finished

Returns whether the project has been loaded completely.

Type

bool

engineering_environment_information

Returns the engineering environment information that includes information which tool was used to last save the project.