Output for error message.
Data type: BOOL
Every error message (Error = TRUE) causes the enable signal at the S_AntivalentOut output to switch to SAFEFALSE and retain this state. The error state (Error = TRUE) can only be exited if there is a valid signal combination at the inputs.
WARNING | |
---|---|
Connection: If required, the signal can be transmitted externally for diagnostic purposes (via a global I/O variable or other functions/function blocks).
Value |
Description |
---|---|
TRUE |
The function block has detected an error. The enable signal at the S_AntivalentOut output switches to SAFEFALSE. |
FALSE |
The function block is either inactive or has not detected an error. |