State-controlled input for the status of the guard locking on the safety equipment. This input processes the feedback signal for locking/unlocking the safety equipment (single-channel or two-channel).
The signal present must be SAFETRUE so that the S_GuardLocked output can be switched to SAFETRUE (taking the other input signals into account).
Data type: SAFEBOOL
Initial value: SAFEFALSE
Connection: Connect this input to the feedback signal of the interlock of the safety equipment, either directly or via other safety-related functions/function blocks. Constant SAFETRUE or SAFEFALSE values are not permitted.
If the function block is activated (input Activate = TRUE), the possible values at this input lead to the following function block behavior:
Value |
Description |
---|---|
SAFETRUE |
The safety equipment is locked. The S_GuardLocked output can now be switched to SAFETRUE, provided that the safety equipment is also closed (S_GuardMonitoring = SAFETRUE), no start-up/restart inhibit is active (S_AutoReset and S_StartReset = SAFEFALSE) and the function block has not detected any errors. Refer to the hazard message below this table. |
SAFEFALSE |
The safety equipment is not locked or the safety equipment wiring has been interrupted or the safety-related input device connected to the safety equipment has been deactivated or is inoperable. If SAFEFALSE is present at the S_GuardLock input, the S_GuardLocked output is always SAFEFALSE, irrespective of all the other input signals. |
If no start-up/restart inhibit has been specified for the function block, the SAFETRUE status at the S_GuardLock input can cause the S_GuardLocked output to immediately switch to SAFETRUE.
WARNING | |
---|---|
Irrespective of whether there is a single-channel or two-channel feedback connection between the guard locking and the Safety Logic Controller, the S_GuardLock input is only connected to one signal.
If a two-channel signal is used, either the input channels of the safety-related input device must be parameterized accordingly or the safety-related SF_Equivalent or SF_Antivalent function block must be connected upstream for evaluation (e.g., SF_Equivalent function block, if the connected switch features two N/C contacts).
Cross-circuit monitoring is not performed by the function block. It is your responsibility to perform this monitoring function outside of this function block in the safety-related control system.