SMC_ABC_SLOPES_NO_STOP (ENUM)

TYPE SMC_ABC_SLOPES_NO_STOP :

Determines how SMC_RecomputeABCSlopes sets the slopes of A/B/C at the transtion between two elements, when there is not stop.

Attributes:

qualified_only

InOut:

Name

Comment

SET_SMOOTH_CARDINAL

The slope at the end of element i is set as (AddAxisValue(i+1) - AddAxisValue(i-1)) / (ElementLength(i) + ElementLength(i+1)). The slope at the start of element i+1 is set to the same value.

DONT_CHANGE

The slope is not changed.