TYPE SMC_M_PARAMETERS : STRUCT
This data type can define additional parameters for the currently active M-function which can be evaluated by SMC_GetMParameters in order to display additional values for the respective M-function.
Name
Type
Initial
dP1
LREAL
0
dP2
dP3
dP4
dP5
dP6
dP7
dP8