SMC_OutQueueInit (FUN)

FUNCTION SMC_OutQueueInit : BOOL

This function intiailizes the SMC_OUTQUEUE.

task-safety: not task-safe; the application has to make sure that no other queue function is called while this function is active, and that no other queue function is active when this function is called.

InOut:

Scope

Name

Type

Comment

Return

SMC_OutQueueInit

BOOL

Input

poq

POINTER TO SMC_OUTQUEUE

Queue to be initialized.