SMC_SegmentAnalyzer (FB)

FUNCTION_BLOCK SMC_SegmentAnalyzer

This function block analyzes the different segments (acceleration constant velocity, deceleration) of a CNC path, independently of the interpolator function block. With every call, the SMC_SegmentAnalyzer outputs basic information about the current path segment and adds up the time that will be needed for its interpolation.

Restrictions:

The complete path must fit into the input path queue. The execution on the output path queue by the next function block (usually SMC_Interpolator ) may only begin, when SMC_SegmentAnalyzer has analyzed the queue completely.

InOut:

Scope

Name

Type

Initial

Comment

Input

bExecute

BOOL

FALSE

With a rising edge, the function block gets active

poqDataIn

POINTER TO SMC_OUTQUEUE

0

Input path queue

iVelMode

SMC_INT_VELMODE

TRAPEZOID

Velocity mode (same as SMC_Interpolator )

dwIpoTime

DWORD

0

Cycle time of the interpolation task (same as SMC_Interpolator )

bMFunctionsPreAcknowledged

BOOL

FALSE

If the input is set to TRUE, every M-function is acknowledged in advance. If the input is set to FALSE, M-functions cause a stop, but they are acknowledged immediately.

dJerkMax

LREAL

0

The magnitude of the maximum allowed jerk (same as SMC_Interpolator ).

Output

bDone

BOOL

FALSE

This output will be set to TRUE as soon as the input data from poqDataIn has been processed completely. The function block will not perform any further actions until it gets reset.

bBusy

BOOL

FALSE

TRUE while execution of function block is not finished

bError

BOOL

FALSE

It signals that an error has occurred within the function block

wErrorID

SMC_ERROR

SMC_NO_ERROR

Error identification:

  • SMC_SA_QUEUE_NOT_IN_BUFFER

  • SMC_SA_QUEUE_CHANGED_DURING_OP

segCurrentSegment

SMC_SEGMENT

Description of the current segment

dTime

LREAL

Total (summed) interpolation time over all segments output so far.

Structure: