SMC_SMOOTHPATHADDAXMODE (ENUM)

TYPE SMC_SMOOTHPATHADDAXMODE :

Mode for handling the additional axes by SMC_SmoothPath

InOut:

Name

Comment

SPAA_LATE

Shift additional axes’ position to end position of inserted spline

SPAA_BROAD

Shift additional axes’ position at the first spline to start, at last spline to the end

SPAA_NONE

Do not consider additional axes

SPAA_EVEN

Distribute positions of additional axes proportional to element lengths

SPAA_EXACT

Cut ABC axes’ position functions like X/Y/Z and connect smoothly