ScriptImagePoolObject

class

ScriptImagePoolObject.

ImageLinkType

value

Bases: Enum

This enumeration represents the way an image is embedded or linked into a project.

Version added

3.5.9.0

Linked

= 1

This value means that the image is linked from the project only.

EmbeddedAndLinked

= 2

This value means that the image is embedded within the project while still linked to the according file in the filesystem and thus allowing automatic updates if changed on disk.

Embedded

= 3

This value means that the image is embedded within the project.

class

ScriptImagePoolObject.

ScriptImagePoolMarker

Bases: object

Marker object to check whether an ScriptObject is an imagepool object.

Version added

3.5.9.0

property

is_imagepool

Gets a value indicating whether this ScriptApplicationMarker is an imagepool.

Return type

bool

Returns

True if it is an imagepool; otherwise, False

class

ScriptImagePoolObject.

ScriptImagePoolObject

Bases: ScriptImagePoolMarker

ScriptObjects which are an imagepool object are extended with this interface.

Version added

3.5.9.0

property

images

Gets the collection of the items currently configured within this imagepool.

Return type

property

download_only_used_images

Gets or sets a value whether all images or only the explicitly referenced ones should be downloaded to PLCs.

Return type

bool

property

imagepool_is_internal

Gets or sets a value whether this image pool is visible for projects embedding the current one as a library.

This is not relevant when working on a project itself.

Return type

bool

property

symboltextlist

Gets and sets the name of the text list for translation of the symbols in this image pool.

Return type

str

class

ScriptImagePoolObject.

ScriptImagePoolItems

iterable=()

/

Bases: list

Gets the current number of items in this image pool.

Version added

3.5.9.0

add

id

path

linktype

updateMode=None

Adds a new image to the current image pool.

Parameters
  • id (str) – The id to assign to the newly inserted image. Must not yet be existing.

  • path (str) – The file path to reference by the new image item.

  • linktype (ImageLinkType) – The way the new image item references the according file.

  • updateMode (AutoUpdateMode) – The way the image item is updated automatically, relevant only if linktype is ImageLinkType.EmbeddedAndLinked

Raises

ArgumentException – Thrown when an item with the according id already existings.

Return type
Returns

The newly created ScriptImagePoolItem.

remove

id

Removes the ScriptImagePoolItem with the given id.

Parameters

id (str) – description

Raises

KeyNotFoundException – Thrown when no entry with the given id exists.

move

indexSrc

indexDst

Moves a ScriptImagePoolItem in the list of items.

Parameters
  • indexSrc (int) – The index of the item that should be moved.

  • indexDst (int) – The index where the item should be located afterwards.

Raises

ArgumentOutOfRangeException – Thrown when the given indices are out of range.

class

ScriptImagePoolObject.

ScriptImagePoolItem

Bases: object

An item (in fact like a line) within a ScriptImagePoolObject.

Version added

3.5.9.0

property

id

The identification of the image that can be accessed in the visualization too.

Raises

ArgumentException – Thrown when the id is being set and the new id is already contained in the imagepool.

Return type

str

property

filepath

The path of the referenced image.

Relevant only if linktype yields ImageLinkType.Linked or ImageLinkType.EmbeddedAndLinked.

Return type

str

property

linktype

The way the image is referenced.

Return type

property

updatemode

The way the image is updated automatically while the project is open.

Relevant only if linktype yields ImageLinkType.EmbeddedAndLinked.

Return type

AutoUpdateMode

class

ScriptImagePoolObject.

ScriptImagePoolObjectContainer

Bases: object

Projects and Application Objects are extended with this interface since CoDeSys V3.5.9.0.

Version added

3.5.9.0

create_imagepool

name=None

Creates a new image pool object in the current context (either application or project global).

Parameters

name (str) – The name of the new imagepool object. In case of None, a default name will be generated.

Raises

ArgumentException – Thrown when an image pool with the given name already exists within the current context.

Return type
Returns

The newly created imagepool object.

get_global_imagepool

Returns the global image pool object or creates a new one if not yet existing.

Typically this method can be called on projects only. Only in case of special customizations of the programming system, it is allowed to call this on an application too.

Raises

InvalidOperationException – Thrown when called on applications when this is not allowed.

Return type
Returns

The global imagepool.

property

has_global_imagepool

Checks whether there is already a globalimagepool in the current location.

Only in case of special customizations of the programming system, it is allowed to call this on an application too.

Raises

InvalidOperationException – Thrown when called on applications when this is not allowed.

Return type

bool