FUNCTION FIND : INT
Searches for the position of a partial string within a string.
FIND(STR1, STR2) means: Find the position of the first character where STR2 appears in STR1 for the first time. If STR2 is not found in STR1, then OUT:=0.
(* Example declaration *)
arINT1 : INT ;
(* Example in ST , result is '4' *)
arINT1 := FIND ('abcdef','de');
| InOut: |
|