FB_Init method used for allocating the memory used for storing the string
InOut:
Scope
Name
Type
Comment
Return
FB_Init
BOOL
Input
bInitRetains
BOOL
bInCopyCode
BOOL
uiBufferSize
UINT
The size of the buffer (in bytes), where the string is stored. If this value is 0, no memory is allocated and the CharBufferPtr pointer has to be set by calling the Initialize method
stringType
__SYSTEM.TYPE_CLASS
A __SYSTEM.TYPE_CLASS value indicating type of the string