METHOD FromString : BOOL
Converts an IEC string value into the internally used representation. The result of the method indicates, whether the processing was successful or not (e.g. CharBufferString.m_Type <> ANY_STRING). If the internally used buffer is not large enough the result is TRUE and only the used buffer size – 1 will be copied.
InOut: |
|